earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, Edge Server, Device Administrator, AS-P
Functionalities: Hardware, License Management
Product version: 2024, 7.0
12/2/2024

Return Demo Licenses on Field Servers

You remove demo licenses from field servers using Device Administrator.

When you return demo licenses from field servers, make sure that you do it with the same demo license file that was used to install the demo licenses.

If you are using a Device Administrator than does not contain the original demo license file, you must do one the following:

  • Add the original demo license file to the Device Administrator you want to use for the return.

  • Rename any demo license file so that it matches the name of the original demo license file that was used when assigned the demo licenses on the field servers. Add the renamed demo license file to Device Administrator.

    If you do not know the name of the demo license file you can log on to the field server with WorkStation. Open System/LicenseManager/LicenseMetadata/ClientMetadata/Product*. The name is in ProductID in the property dialog box for the demo license file object.

For more information, see Removing Demo Licenses File from Device Administrator .

  • Demo Licensing Overview
  • Field Server Demo License Management
  • Returning All Demo Licenses from the Selected Field Servers
  • Return Demo Licenses from Field Servers Workflow