earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-B, Edge Server, Device Administrator, AS-P
功能: 硬件, 许可证管理
产品版本: 2023
2023/2/13

Return Demo Licenses on Automation Servers

You remove demo licenses from automation server using Device Administrator.

When you return demo licenses from automation servers, make sure that you do it with the same demo license file that was used to install the demo licenses.

If you are using a Device Administrator than does not contain the original demo license file, you must do one the following:

  • Add the original demo license file to the Device Administrator you want to use for the return.

  • Rename any demo license file so that it matches the name of the original demo license file that was used when assigned the demo licenses on the automation servers. Add the renamed demo license file to Device Administrator.

    If you do not know the name of the demo license file you can log on to the automation server with WorkStation. Open System/LicenseManager/LicenseMetadata/ClientMetadata/Product*. The name is in ProductID in the property dialog box for the demo license file object.

有关更多信息,请参阅 Removing Demo Licenses File from Device Administrator .

  • Demo Licensing Overview
  • SpaceLogic Automation Server Demo License Management
  • Returning All Demo Licenses from the Selected SpaceLogic Automation Servers
  • Return Demo Licenses from SpaceLogic Automation Servers Workflow