earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-B, Edge Server, Device Administrator, AS-P
功能: 硬件, 许可证管理
产品版本: 2023
2023/6/20

Return Licenses on SpaceLogic Automation Servers

You can return licenses from automation servers.

This is done, for example, if you for some reasons have assign and activated licenses on an automation server that does not need licenses. When the licenses have been returned they can be used on another automation server.

Returning licenses on automation servers requires that the automation servers or the computer that runs Device Administrator is connected to the Internet.

When you return licenses, all licenses on the selected server are returned.

  • Automation Server Licensing Overview
  • Returning Licenses on Automation Servers