earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Poradnik

Poradnik


Produkty: AS-B, Device Administrator, AS-P
Funkcje: Sprzęt, Zarządzanie licencją
Wersja produktu: 2022
2025-02-26

Returning Licenses on SpaceLogic Automation Servers

You return licenses so that they can be used elsewhere.

Pokaż więcej
action_close

You can return licenses from automation servers.

This is done, for example, if you for some reasons have assign and activated licenses on an automation server that does not need licenses. When the licenses have been returned they can be used on another automation server.

Licenses can only be returned if the automation server is online.

When you return licenses, all licenses on the selected server are returned.

To return Licenses on SpaceLogic automation servers
  1. In Device Administrator, click Servers .

  2. Select Show licenses .

  3. Select the automation servers where you want to return the licenses.

  4. Click Other .

  5. Click Return licenses .

  6. In the Return All Licenses dialog box, click Yes .

  • Automation Server Licensing Overview
  • Return Licenses on SpaceLogic Automation Servers
  • Other Menu