earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Пользовательский интерфейс

Пользовательский интерфейс


Продукты: AS-B, Edge Server, Device Administrator, AS-P
Функции: Аппаратное обеспечение, Управление лицензиями
Версия продукта: 2024, 7.0
03.12.2024

Add Entitlement from ID

Use the Add Entitlement from ID dialog box to add the entitlement ID when the entitlement certificate HTML-file is not available.

 
action_zoom_plus_stroke Add Entitlement from ID dialog box
Рисунок: Add Entitlement from ID dialog box

Таблица: Add Entitlement from ID Dialog Box

Command

Description

Entitlement ID

Enter the entitlement ID provided in the confirmation e-mail of your product purchase.

  • Field Server Licensing on Field Servers Connected to Internet Workflow
  • Field Server Licensing on Field Servers not Connected to Internet Workflow
  • Restarting Field Servers from Device Administrator
  • Add Entitlement from File
  • Checking Entitlement Dialog Box
  • Contacting License Activation Server Dialog Box