earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B, Edge Server, Device Administrator, AS-P
功能: 硬件, 许可证管理
产品版本: 2024, 7.0
2024/12/3

Add Entitlement from File

Use the Add Entitlement from file dialog box to add the entitlement.

 
action_zoom_plus_stroke Add Entitlement from file dialog box
图: Add Entitlement from file dialog box

表格: Add Entitlement from File Dialog Box

Command

Description

Browse

Browse to the entitlement file.

  • Field Server Licensing on Field Servers Connected to Internet Workflow
  • Field Server Licensing on Field Servers not Connected to Internet Workflow
  • Restarting Field Servers from Device Administrator
  • Add Entitlement from ID
  • Checking Entitlement Dialog Box
  • Contacting License Activation Server Dialog Box