earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Пользовательский интерфейс

Пользовательский интерфейс


Продукты: AS-B, Edge Server, Device Administrator, AS-P
Функции: Безопасность
Версия продукта: 2024, 7.0
02.12.2024

Invalid Certificate Dialog Box

Use the Invalid Certificate dialog box to temporarily trust an invalid certificate.

 
action_zoom_plus_stroke Invalid Certificate dialog box
Рисунок: Invalid Certificate dialog box

Таблица: Invalid Certificate Dialog Box

Component

Description

Do not trust the certificate

Select if you do not trust the certificate.

Trust the certificate

Select to temporarily trust an invalid certificate when you are sure that you have a secure connection between Device Administrator and the field server.

  • Certificate State
  • Certificates Managed using Device Administrator