earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: RP-C
Functionalities: Hardware
Product version: 2023, 2024, 7.0
3/30/2023

RP-C Communication Ports

The RP controller provides a combination of communication ports, such as:

  • Ethernet port(s)

  • USB port(s)

  • RS-485 port(s)

The number and types of communication ports differ between the different controller models.

Regarding the differences in the set of communcation ports, the RP-C models can be divided into the following three categories:

  • Models with “-F” in the product name:

    RP-C-12A-F-24V, RP-C-12B-F-24V, RP-C-12C-F-24V, RP-C-16A-F-230V, RP-C-16B-F-24V, and RP-C-16B-F-230V

  • RP-C-16C-F-230V model

  • Models with “-M” in the product name:

    RP-C-12A-M-24V, RP-C-12B-M-24V, and RP-C-16A-M-24V

For more information, see RP-C Models .

Communication Ports on RP-C Models with “-F” in the Product Name

The RP-C provides the following combination of communication ports:

  • Two Ethernet ports

  • Two USB ports

  • Two RS-485 ports (RJ45)

For more information, see Communication Ports on RP-C Models with “-F” in the Product Name .

Communication Ports on RP-C-16C-F-230V

The RP-C provides the following combination of communication ports:

  • Two Ethernet ports

  • One USB port

  • Three RS-485 ports (RJ45)

For more information, see Communication Ports on RP-C-16C-F-230V .

Communication Ports on RP-C Models with “-M” in the Product Name

The RP-C provides the following communication ports:

  • One RS-485 port with RJ45 interface

  • One RS-485 port with terminal block

For more information, see Communication Ports on RP-C Models with “-M” in the Product Name .

  • RP-C Controllers
  • RP-C Models
  • Communication Ports on RP-C Models with “-F” in the Product Name
  • Communication Ports on RP-C-16C-F-230V
  • Communication Ports on RP-C Models with “-M” in the Product Name