earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Концепт

Концепт


Продукты: RP-IO
Функции: Аппаратное обеспечение
Версия продукта: 2023, 2024, 7.0
12.12.2023

RP-IO Module LED

arrow1_rotationStatus LED

There is one LED on the front panel of the RP-IO module.

 
action_zoom_plus_stroke RP-IO module LED
Рисунок: RP-IO module LED

Таблица: RP-IO Module LED

Function

Color

Status

Red, Green, Blue (and combinations)

Status LED

The RP-IO module Status LED indicates the condition of the device.

Таблица: RP-IO Module Status LED Patterns

LED Patterns

Condition

Green, constant

Normal operation, status OK

RP-IO module firmware application running

Green 3 seconds, blue 1 second

Normal operation, status OK

RP-IO module firmware application running

Green, flashing (~1 Hz)

Device restarting, wait

RP-IO module firmware application running

Red, constant

Detected error, attention required

Red, flashing (~1 Hz)

Device operates, but a problem needs attention

Red/green, flashing (~1 Hz)

RP I/O board receiving software upgrade, wait

Do not interrupt power to the controller. For more information, see the following Important note.

Amber, constant

RP-IO module firmware boot applet running

Amber, flash

Device restarting, wait

RP-IO module firmware boot applet started

Amber/green, flashing (~1 Hz)

RP-IO module firmware is being upgraded. It is typically the firmware main application, but it can also be a boot applet.

White, transient

Device starting, wait

White, constant

RP-IO module firmware not running, attention required (contact product support)

Примечание

Avoid power interruptions to the device during the brief period when the Status LED is flashing red and green. An interruption causes problems with the I/O processor upgrade and can result in corrupt firmware. You can view the evidence of a corrupt processor when the device reports itself as an “MP-C-15A.” A corrupt I/O processor can lead to the loss of the reset button and/or I/O functionality, as well as the inability to upgrade the I/O processor and/or the device.

  • RP-IO Modules
  • RP-IO Models
  • Status LEDs