earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Comment faire pour

Comment faire pour


Produits : AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Fonctionnalités : Semantic
Version produit : 2023
07/02/2023

Creating Tenant Repositories on the Semantic Database

You create the tenant on the semantic database so that the tenant repositories you created on the EcoStruxure Building Operation server is uploaded to the semantic database.

Afficher plus
action_close

The EcoStruxure Building Operation software supports a database solution for external storage of semantic information.

The semantic information is a contextual representation of a building that follows the Brick schema. It includes representation of building assets such as points, locations, and equipment.

The semantic information is configured in WorkStation, and the information is available in WorkStation and WebStation. The information is also available through EcoStruxure Web Services.

Semantic Database

EcoStruxure Building Operation uses a Sparql database, GraphDB from Ontotext, to handle semantic queries.

Pour plus d'informations, voir Semantic Database .

Ontologies

Semantic is based on ontologies.

Pour plus d'informations, voir Ontologies .

Semantic Data and EWS

The EWS metadata makes it possible to add semantic information to the EWS items, provided that the EBO object that is exposed by EWS is semantically described.

Semantic tagging is exposed using EWS.

Pour plus d'informations, voir Semantic Data and EWS .

Licensing

You can use a limited number of queries in the Graph database without a license. To be able to use the Graph database to its full extent a license is needed.

If you use an GraphDB on another location than the EBO default location, you have to aquire a license.

Semantic Navigation

You can navigate the semantic database using search and filter.

Pour plus d'informations, voir Semantic Navigation in WorkStation .

Pour plus d'informations, voir Semantic Navigation in WebStation .

Configure EcoStruxure Building Automation System to use Semantic Tagging

Use this workflow to configure EcoStruxure Building Automation system to use semantics.

Pour plus d'informations, voir Configure EcoStruxure Building Automation System to use Semantic Workflow .

Semantic Engineering

Semantic engineering is the process describing an EcoStruxure Building operation database using semantic s .

Pour plus d'informations, voir Semantic Engineering Overview .

Tenant Repository

You can create a semantic repository for each tenant. You do this in a system with multi tenants where you do not want the tenants to share their semantic information.

Pour plus d'informations, voir Tenant Repository .

To create tenant repositories on the semantic database
  1. In WorkStation, in the System Tree pane, in the System folder, expand Semantics .

  2. Right-click Tenant repositories and then click Create tenant repositories .

The tenant repositories are created on the semantic database.

  • Semantic Overview
  • Semantic Engineering Overview
  • Semantic Tenant Repository Workflow
  • Tenant Repository
  • Tenant Repositories Dialog Box
  • Tenant Repository Dialog Box
  • Populating a Tenant Repository
  • Connecting a User Group to the Tenant Repository