earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Security
Product version: 2024, 7.0
12/2/2024

WorkStation Generate Certificate Workflow

Use this workflow to generate and activate a certificate using WorkStation.

Related information can be found in the sections after the flowchart.

 
action_zoom_plus_stroke Server certificate workflow
Figure: Server certificate workflow
Generate the certificate

Generate the certificate using WorkStation.

For more information, see Generating a Certificate Using WorkStation .

Activate the certificate

Activate the certificate on the EcoStruxure BMS server.

For more information, see Activating a Certificate Using WorkStation .

Verify the Connection

Verify that the connection to WebStation is secure by accessing the EcoStruxure BMS server via HTTPS.

  • Certificates
  • Generating a Certificate Using WorkStation
  • Activating a Certificate Using WorkStation