earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: MP-C
功能: 硬件
产品版本: 2023, 2024, 7.0
2023/6/20

Communication Ports on MP-C-24A-M and -36A-M

The MP-C provides the following communication port:

  • One RS-485 port with terminal block

The RS-485 port with screw terminal block is used for connection to the BACnet MS/TP (RS-485) network.

The screw terminals are labeled:

  • RS-485+

  • RS-485–

  • Shield

有关更多信息,请参阅 MP-C-24A-M Screw Terminals .

有关更多信息,请参阅 MP-C-36A-M Screw Terminals .

有关更多信息,请参阅 RS-485 Communications .

  • Hardware Overview
  • MP-C Controllers
  • MP-C-24A-M Screw Terminals
  • MP-C-36A-M Screw Terminals
  • RS-485 Communications