earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Produits : MP-C
Fonctionnalités : Matériel
Version produit : 2023, 2024, 7.0
20/06/2023

MP-C Communication Ports

The MP-C controller provides a combination of communication ports, such as:

  • Ethernet port(s)

  • USB port(s)

  • RS-485 port(s)

The number and types of communication ports differ between the different controller models.

Regarding the differences in the set of communcation ports, the MP-C models can be divided into the following two categories:

  • Models without “-M” in the product name: MP-C-15A, MP-C-18A, MP-C-18B, MP-C-24A, and MP-C-36A

  • Models with “-M” in the product name: MP-C-24A-M and MP-C-36A-M

Pour plus d'informations, voir MP-C Models .

Communication Ports on MP-C-15A, -18A, -18B, -24A, and -36A

The MP-C provides the following combination of communication ports:

  • Two Ethernet ports

  • Two USB ports

  • One RS-485 port

Pour plus d'informations, voir Communication Ports on MP-C-15A, -18A, -18B, -24A, and -36A .

Communication Ports on MP-C-24A-M and -36A-M

The MP-C provides the following communication port:

  • One RS-485 port with terminal block

Pour plus d'informations, voir Communication Ports on MP-C-24A-M and -36A-M .

  • MP-C Controllers
  • MP-C Models
  • Communication Ports on MP-C-15A, -18A, -18B, -24A, and -36A
  • Communication Ports on MP-C-24A-M and -36A-M