The MP-C controller provides a combination of communication ports, such as:
Ethernet port(s)
USB port(s)
RS-485 port(s)
The number and types of communication ports differ between the different controller models.
Regarding the differences in the set of communcation ports, the MP-C models can be divided into the following two categories:
Models without “-M” in the product name: MP-C-15A, MP-C-18A, MP-C-18B, MP-C-24A, and MP-C-36A
Models with “-M” in the product name: MP-C-24A-M and MP-C-36A-M
Mer information finns i MP-C Models .
The MP-C provides the following combination of communication ports:
Two Ethernet ports
Two USB ports
One RS-485 port
Mer information finns i Communication Ports on MP-C-15A, -18A, -18B, -24A, and -36A .
The MP-C provides the following communication port:
One RS-485 port with terminal block
Mer information finns i Communication Ports on MP-C-24A-M and -36A-M .