earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Как

Как


Продукты: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Функции: Базовые функции
Версия продукта: 2024, 7.0
02.12.2024

Uploading and Downloading a Backup using WebStation

You can upload and download a backup using WebStation.

Показать больше
action_close

A subset of backup and restore features are available in WebStation.

You can create backups of the server using WebStation. The backup can be downloaded and uploaded from the server.

Scheduled backup must be done using WorkStation.

Более подробную информацию см. Backup .

To upload and download a backup using WebStation
  1. Click WebStation, click Workspace menu .

  2. Click System .

  3. Click Backup and restore .

  4. In the Backup and restore dialog:

    • Click Upload to upload a backup.

    • Select a backup and click Download to download the selected backup.

  • Backup and Restore Overview
  • Backup and Restore using WebStation
  • Backing up and Restoring using WebStation
  • Backup