earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 基本功能
产品版本: 2024, 7.0
2024/12/2

Uploading and Downloading a Backup using WebStation

You can upload and download a backup using WebStation.

显示更多
action_close

A subset of backup and restore features are available in WebStation.

You can create backups of the server using WebStation. The backup can be downloaded and uploaded from the server.

Scheduled backup must be done using WorkStation.

有关更多信息,请参阅 Backup .

To upload and download a backup using WebStation
  1. Click WebStation, click Workspace menu .

  2. Click System .

  3. Click Backup and restore .

  4. In the Backup and restore dialog:

    • Click Upload to upload a backup.

    • Select a backup and click Download to download the selected backup.

  • Backup and Restore Overview
  • Backup and Restore using WebStation
  • Backing up and Restoring using WebStation
  • Backup