earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
5
概念

概念


产品: MP-C
功能: 硬件
产品版本: 2023, 2024, 7.0
2023/6/20

RJ45 Pinout for the RS-485 Port of the MP-C Controller

This section provides the RJ45 pinout for the MP-C controller's RS-485 port.

The number of RS-485 ports with RJ45 interface differ between the different controller models.

Regarding the differences in the set of RS-485 ports, the MP-C models can be divided into the following two categories:

  • Models without “-M” in the product name:

    MP-C-15A, MP-C-18A, MP-C-18B, MP-C-24A, and MP-C-36A

  • Models with “-M” in the product name:

    MP-C-24A-M and MP-C-36A-M

有关更多信息,请参阅 MP-C Models .

The MP-C-15A, -18A, -18B, -24A, and -36A models have one RS-485 port with RJ45 interface, which is labeled RS-485 Com A.

The MP-C-24A-M and -36A-M models have no RS-485 port with RJ45 interface.

The wiring recommendations for the RS-485 port depend on the type of network the port iss are used for. 有关更多信息,请参阅 Communication Port Wiring .

 
action_zoom_plus_stroke RJ45 pinout for the RS-485 port of the MP-C controller
图: RJ45 pinout for the RS-485 port of the MP-C controller

表格: RJ45 Pinout for the RS-485 Com A Port

RJ45 Pin

Description

1

Not connected

2

Not connected

3

RS485+ (A)

4

+24 VDC

5

Ground

6

RS485– (B)

7

+24 VDC

8

Ground

  • Wiring
  • Communication Port Wiring
  • MP-C Communication Ports
  • Communication Ports on MP-C-15A, -18A, -18B, -24A, and -36A
  • Communication Ports on MP-C-24A-M and -36A-M
  • MP-C Sensor Bus
  • MP-C Modbus
  • MP-C Models