earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Pojęcie

Pojęcie


Produkty: Operator Display
Funkcje: Podstawowa funkcjonalność
Wersja produktu: 3.3, 2022, 2023, 2024, 7.0
2023-04-24

Configuration Menus

Configuration Menus are a group of pre-engineered objects and values that can customize and simplify the information that is displayed on devices. When Configuration Menus exist in the connected RP-C or MP-C Controller, Operator Display will show these menus in place of the default input/output value menus.

Uwaga

Alarm and schedule menus will still be displayed when Configuration Menus are present.

EcoStruxure Building Operation - Technical Reference Guide

Overview

You use configuration menus to customize values shown on Operator Display.

You create the configuration menu in Configuration Menu Editor to contain any source values presented by Operator Display. The menu is deployed to the RP-C or MP-C Controller and can then be accessed with Configuration Menu Viewer in Workstation, a Commission mobile application or Operator Display.

There are no limitations on the size of menus, but it is recommended to not build extensive menus to simplify its use for the devices.

Operator Display will show a maximum of 16 Configuration Menus per RP-C/MP-C Controllers.

Configuration Menu Editor

You use Configuration Menu Editor to design a menu to display, and then configure, source values presented by Operator Display.

EcoStruxure Building Operation - Technical Reference Guide