earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WebStation
Functionalities: Dashboards
Product version: 2024, 7.0
12/10/2024

Image Widget Dialog Box

Use the Image Widget dialog box to add or replace an image.

 
action_zoom_plus_stroke Image widget dialog box
Figure: Image widget dialog box

Table: Image Widget Dialog Box

Component

Description

Image

Browse to the image you want to display in the image widget.

Image Stretch

Select how you want the image to be displayed in the image widget.

  • Select Cover to fit the image into the image widget without any resizing.

  • Select Fit to adjust the image to fit in the image widget. The image is resized without losing its proportions.

  • Select Fill to adjust the image to fit in the image widget. The image is resized and lose its proportions.

  • How Dashboards Work
  • Dashboard Widgets
  • Image Widget
  • Widget Dialog Box – Layout Tab