earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Device Administrator, ​License Administrator, AS-P
功能: 硬件, SmartDriver
产品版本: 2024, 7.0
2024/12/2

Sending the Response Files to the Selected Field Server when Returning Licenses

You send the response files from License Activation Server (FNO) to the field server when you want to return licenses.

You gather, and download, the license information from the field servers. This information is used to identify the licenses that is to be reclaimed from the License Activation Server (FNO).

显示更多
action_close

Device Administrator is used to manage licenses on field servers.

Software and Features that Require Licenses

A number of software features need licenses.

有关更多信息,请参阅 Software and Features that Require Licenses .

Entitlements, Products, and Licenses

Licenses are bought as products and delivered in Entitlements. An Entitlement is a container that can contain several products. The products contain the licenses and they can differ in quantity and contents.

Field Server Licensing Workflow

Use one of these workflows, depending on if the field servers are connected or not connected to the Internet.

有关更多信息,请参阅 Field Server Licensing on Field Servers Connected to Internet Workflow .

有关更多信息,请参阅 Field Server Licensing on Field Servers not Connected to Internet Workflow .

Certificates

It is recommended to use HTTPS for the communication between Device Administrator and field servers when you manage licenses.

有关更多信息,请参阅 Certificates Managed using Device Administrator .

Return Licenses on Field Servers

You can return licenses from field servers.

有关更多信息,请参阅 Return Licenses on Field Servers .

To send the response files to the selected field server when returning licenses
  1. In Device Administrator, click Servers .

  2. Select Show Licenses .

  3. Select the field servers.

  4. Click Return .

  5. Click Send response files to the selected automation servers .

  6. Click OK .

  7. In the Response field, browse to the response file.

  8. In the Confirmation field, browse to the location where you want to save the confirmation files.

  9. Click OK .

  • Field Server Licensing Overview
  • Field Server Licensing on Field Servers Connected to Internet Workflow
  • Field Server Licensing on Field Servers not Connected to Internet Workflow
  • Activate Licenses Offline Dialog Box
  • Assigning Licenses