earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Пользовательский интерфейс

Пользовательский интерфейс


Продукты: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool, WebStation
Функции: Dashboards, Sustainability
Версия продукта: 2024, 7.0
10.12.2024

Consumption Signature Widget Dialog Box

Use the Consumption Signature Widget dialog box to configure and edit a consumption signature.

 
action_zoom_plus_stroke Consumption siganture widget dialog box
Рисунок: Consumption siganture widget dialog box

Таблица: Consumption Signature Widget Dialog Box

Component

Description

Signature object

Select the column(s) you want to display in the widget.

Expected color

Select the filter you want to apply.

Actual color

Enter the number of bars you want to display in the chart.

Y-axis minimum

Enter the Y-axis minimum.

Y-axis maximum

Enter the Y-axis maximum.

Decimals

Select the number of decimals you want to display.

Period

Select the period you want to display.

Caption

Type a caption for the widget.

Caption link

Select to make a link to an object that is relevant to the values that are displayed in the widget.

Show legend

Click True to display the name and color of the trend log in the widget.

Show alarm limits

Click True to show alarm limits.

Show gridlines

Click True to show gridlines.

Show period

Click True to show period.

  • How Dashboards Work
  • Dashboard Widgets
  • Widget Dialog Box – Layout Tab