earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Пользовательский интерфейс

Пользовательский интерфейс


Продукты: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool, WebStation
Функции: Dashboards, Sustainability
Версия продукта: 2024, 7.0
10.12.2024

Consumption Signature Plot Widget Dialog Box

Use the Consumption Signature Plot Widget dialog box to configure and edit a consumption signature plot widget.

 
action_zoom_plus_stroke Consumption signature plot widget dialog box
Рисунок: Consumption signature plot widget dialog box

Таблица: Consumption Siganture Plot Widget Dialog Box

Component

Description

Signature object

Select the consumption signature you want to display in the widget.

Highlighted dates

Select a calendar that defines the day that have a differnt color from the one in the signature curve.

Highlight color

Enter the number of bars you want to display in the chart.

Show highlight as heatmap

Select True to display the plotted information as a heat map.

X -axis minimum

Enter the Y-axis minimum.

X-axis maximum

Enter the Y-axis maximum.

Y-axis minimum

Enter the Y-axis minimum.

Y-axis maximum

Enter the Y-axis maximum.

Decimals

Select the number of decimals you want to display.

Caption

Type a caption for the widget.

Caption link

Select to make a link to an object that is relevant to the values that are displayed in the widget.

Show legend

Click True to display the name and color of the trend log in the widget.

Show alarm limits

Click True to show alarm limits.

Alarm limit color

Select the color for the alarm limits.

Show expected line

Select True to display the expected consumption signature line.

Show gridlines

Click True to show gridlines.

Show period

Click True to show period.

  • Dashboard Widgets
  • XY Plot
  • Widget Dialog Box – Layout Tab