Use the Meter object – Basic tab to configure the meter object settings.
Property |
Description |
Status |
Displays the status of the monitored value. Read-only. For more information, see Meter Status and Meter Mode . |
Mode |
Displays the mode of the monitored value. Read-only. For more information, see Meter Status and Meter Mode . |
Meter unit |
Select the preferred unit. For more information, see Meter Object Unit . |
Monitored variable (kWh) |
Enter the physical meter you want to monitor. |
Max value (kWh) |
Enter the max value the physical meter can hold until it rolls over. |
Interval (ms) |
Enter the log interval. |
Log size |
Enter the log size. |