earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Пользовательский интерфейс

Пользовательский интерфейс


Продукты: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Функции: Sustainability
Версия продукта: 2024, 7.0
23.02.2024

Meter Processor Properties – Input Dialog Box

Use the Meter Processor Properties – Input dialog box to add and calculate values from a meter object or a meter processor to a meter processor.

 
action_zoom_plus_stroke Meter processor properties – Input dialog box
Рисунок: Meter processor properties – Input dialog box

Таблица: Meter Processor Properties – Input Dialog Box

Property

Description

Meter

Select the meter object or meter processor you want to add to your meter processor.

Contribution

Select Add to add the meter object value to the meter process output.

Select Subtract to subtract the meter object value from the meter process output.

Percentage

Select the contribution in percentage.

  • Meter Processor
  • Meter Processor – Basic Tab