earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Концепт

Концепт


Продукты: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Функции: Sustainability
Версия продукта: 2024, 7.0
23.02.2024

Meter Object

arrow1_rotationAdjusted Meter Value arrow1_rotationMeter Object Unit arrow1_rotationMeter Replacement arrow1_rotationReset Meter Object arrow1_rotationUnexpected Meter Object Values arrow1_rotationBuilt in Meter Log

The meter object is used to log and calculate values from a physical meter using a point, called monitored variable, in the EBO server. The monitored variable can, for example, be a Modbus point or a BACnet point.

 
action_zoom_plus_stroke Meter Object
Рисунок: Meter Object

Adjusted Meter Value

To get correct values in the meter object, the meter value in the meter object must be configured to handle for example meter roll over.

Более подробную информацию см. Adjusted Meter Value .

Meter Object Unit

The unit in the meter object is used for calculated consumption, logging and maximum setting for meter roll over on the physical meter. To get correct values in the meter object, the monitored variable must have the same unit as the active energy unit in the physical meter.

Более подробную информацию см. Meter Object Unit .

Meter Replacement

When you replace a physical meter, you need to make adjustment to the meter object that monitor the physical meter.

Более подробную информацию см. Meter Replacement .

Reset Meter Object

Meter objects can be reset. This is typically done after you have tested a meter object configuration or when you want to restart the calculation and logging in a meter object.

Более подробную информацию см. Reset a Meter Object .

Unexpected Meter Object Values

The meter object can take different status and modes.

Более подробную информацию см. Meter Status and Meter Mode .

Built in Meter Log

The meter object has a built in meter log. The meter log logs the output of the meter object. A meter log can be presented in a trend chart or in a trend log list.

Use the calculation method Delta when you want to show consumption over periods in Dashboards, trend log lists and trend charts.

  • Meter Object Unit
  • Adjusted Meter Value
  • Meter Replacement
  • Reset a Meter Object
  • Meter Status and Meter Mode