Funktionaliteter: Sustainability
Produktversion: 2024
2024-12-04

Resetting a Meter Object

You reset a meter object, for example, after a testing. After the reset the meter object restart calculations and logging.

Visa mer
action_close

Meter objects can be reset. This is typically done after you have tested a meter object configuration or when you want to restart the calculation and logging in a meter object.

When you reset the meter object, the meter object log is cleared and the meter value and the calculated consumption is set to 0. The meter object then restart calculation and logging.

You can reset multiple meter objects at the same time using Search and mass editing.

Mer information finns i Search Overview .

Mer information finns i Mass Editing Objects .

To reset a meter object
  • Do one of the following:

    • In WorkStation, right-click the meter object, point to Meter management then click Reset meter value .

    • In WebStation, right-click the meter object, then click Reset meter value .

  • Meter Object
  • Reset a Meter Object