earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: Sustainability
产品版本: 7.0
2025/7/2

Resetting a Meter Object

You reset a meter object, for example, after a testing. After the reset the meter object restart calculations and logging.

显示更多
action_close

Meter objects can be reset. This is typically done after you have tested a meter object configuration or when you want to restart the calculation and logging in a meter object.

When you reset the meter object, the meter object log is cleared and the calculated consumption is set to 0. The meter object then restart calculation and logging.

You can reset multiple meter objects at the same time using Search and mass editing.

有关更多信息,请参阅 Search Overview .

有关更多信息,请参阅 Mass Editing Objects .

To reset a meter object
  • Do one of the following:

    • In WorkStation, right-click the meter object, point to Meter management then click Reset consumption value and clear trend log . In the Reset dialog, click Yes .

    • In WebStation, right-click the meter object, then click Reset consumption value and clear trend log . In the Reset meter dialog, click Reset meter .

  • Meter Object
  • Reset a Meter Object