earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Sustainability
Product version: 2024, 7.0
2/23/2024

Meter Replacement Workflow

The following flowchart shows the tasks for replacing a meter. Related information can be found in the sections after the flowchart.

 
action_zoom_plus_stroke Meter replacement workflow
Figure: Meter replacement workflow
Initiate the meter replacement

Set the meter object in replacement mode. The meter object pauses the calculations and the updates of meter values when in replacement mode.

For more information, see Initiating a Meter Replacement .

Replace the meter

Replace the physical meter.

Finalize the meter replacement

Update the configuration of the monitored variable if the new physical meter is exposed using a different address or register.

Complete the meter replacement by finalizing the meter replacement.

For more information, see Finalizing a Meter Replacement .

Finalizing opens the Manage Replacement of Meter dialog box where you specify the final value of the old physical meter and the start value and maximum value of the new physical meter.

For more information, see Manage Replacement of Meter Dialog Box .

  • Meter Object
  • Meter Replacement
  • Initiating a Meter Replacement
  • Finalizing a Meter Replacement
  • Manage Replacement of Meter Dialog Box