Funktionaliteter: Sustainability
Produktversion: 2024, 7.0
2024-02-23

Meter Status and Meter Mode

arrow1_rotationMeter Status arrow1_rotationMeter Mode

The meter object can take different status and modes.

Meter Status

The meter object can be in two states, OK or an error state.

Meter Mode

The meter object can be in the following modes:

Normal

The meter object works as expected. It logs and calculates consumption.

Meter Replacement

A meter replacement is initiated.

Mer information finns i Meter Replacement .

Unexpected Meter Values

When an unexpected value is detected, the meter object enters the mode Action needed and the status of the meter object is set to inform the user that something unexpected happened.

A meter object in Action needed mode pauses the calculations and does not update the meter values.

You start the meter object again with the command Confirm meter setting .

Mer information finns i Confirming a Meter Object Settings .

The command Confirm meter settings open a dialog where you can change the maximum settings and set the start value of the connected meter. For example, if the mode Action needed was caused by an unexpected meter replacement.

  • Meter Object
  • Meter Replacement
  • Confirming a Meter Object Settings