earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Концепт

Концепт


Продукты: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Функции: Sustainability
Версия продукта: 2024, 7.0
23.02.2024

Meter Processor Charts

You can display a chart in WebStation that shows how much each connected meter object, or meter processor, contributes to the calculated result.

The values in the charts are the calculated consumption values of the meter processor and its connected meter objects and meter processors. The values are runtime variables, not logged values. You can choose to view this hour, today, this week, this month, or this year in the toolbar. Default view is today.

Type of charts

You can choose the following type of charts:

  • Sankey

  • Pie

  • Sunburst

The charts cannot visualize negative values from the connected meter objects and meter processors. You get negative values when you use Contribution=Subtract.

Hierarchy display

The pie chart only displays the contribution of the connected meter objects and meter processors, while the Sankey chart and sunburst charts also show the meter hierarchy, with the selected meter processor as the root of the hierarchy.

  • Meter Processor
  • Viewing a Meter Processor Chart