earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Как

Как


Продукты: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool, WebStation
Функции: Dashboards, Sustainability
Версия продукта: 2024
23.02.2024

Configuring a Consumption Signature Plot Widget

The consumption signature object is used to calculate, analyze, and graphically present expected energy consumption.

Показать больше
action_close

A consumption signature plot is an XY plot similar to the configuration tool. The plot can show the alarm limits and you can also connect a calendar to highlight values for certain days in the plot. Highlighted values can be plotted or represented by a heatmap.

To configure a consumption signature plot widget
  1. Right-click the dashboard and click Edit dashboard .

  2. Click Configure or click the Settings button

     
    action_zoom_plus_stroke
    .

  3. In the Signature object , select the object you want to display in the plot.

  4. In the Highlighted dates , select the calendar which includes the days you want to highlight

  5. Select the color to use for the highlight dates.

  6. Select to show the highligt as a heatmap.

  7. In the X-axis maximum box, enter the maximum value of the left x-axis.

  8. In the X-axis minimum box, enter the minimum value of the x-axis.

  9. In the Y-axis minimum box, enter the minimum value of the y-axis.

  10. In the Y-axis maximum box, enter the maximum value of the y-axis.

  11. In the Decimal box, select the number of decimals to display.

  12. In the Period box, select a period.

  13. In the Caption box, type a caption.

  14. In the Caption link box, enter a link to an object that is relevant for the point gauge.

  15. In the Show Legend box, select True to display legends in the chart.

  16. In the Show alarm limits box, select True to display the alarm limits.

  17. In the Show gridlines box, select True to display gridlines.

  18. Select to show the period.

  19. Click OK .

  • Dashboard Widgets
  • Consumption Signature Plot Widget
  • Consumption Signature Plot Widget Dialog Box