earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Пользовательский интерфейс

Пользовательский интерфейс


Продукты: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Функции: Безопасность
Версия продукта: 2024, 7.0
10.12.2024

Web Server Certificate Dialog Box – Basic Tab

Use the Web Server Certificate dialog box basic tab to connect to the Enrollment over Secure Transport server and to add Certificate Signing Request (CSR) information.

 
action_zoom_plus_stroke Web Server Certificate dialog box
Рисунок: Web Server Certificate dialog box

Таблица: Web Server Certificate Dialog Box

Component

Description

Enabled

Select Yes to enable the certificate agent.

CSR information

Type a string for adding information to the CSR specified as a string consisting of a sequence of attribute type and value pairs separated by a semicolon (;). The general form is <type>=<value>(;<type>=<value>)*[;]

  • Public Key Infrastructure in EcoStruxure Building Operation
  • PKI Settings Dialog Box – Basic Tab