You configure the global certificate settings so that the EcoStruxure Building Operation servers can communicate with the PKI server using EST.
In WorkStation, in the System Tree pane, expand System .
Expand Security Manager .
Click PKI Settings .
Click Properties .
Click the Basic tab.
Configure the settings. For more information, see PKI Settings Dialog Box – Basic Tab .
Click Save .
You can configure multiple servers at the same time using search and mass editing.
For more information, see Search Overview .
For more information, see Mass Editing Objects .