earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 安全
产品版本: 2024
2024/2/22

PKI Settings Dialog Box – Basic Tab

Use the PKI Settings dialog box – basic tab to configure the global certificate settings so that the EcoStruxure Building Operation servers can communicate with the PKI server using EST.

 
action_zoom_plus_stroke PKI Settings dialog box – basic tab
图: PKI Settings dialog box – basic tab

表格: PKI Settings Dialog Box – Basic Tab

Component

Description

EST server address

Type the address to the PKI server that is using the EST protocol.

EST server port

Enter the PKI server port.

Trust anchor filename

Browse to the file that contains the PEM-formatted CAs and intermediate certificates that are utilized during the initial handshake to establish trust.

Proxy address

Type the address to the proxy.

Proxy port

Select the proxy port.

Username

Type the username for the authentication.

Password

Type the password for the user.

Confirm password

Confirm the password for the user.

Client certificate filename

Browse to the client certificate file when certificate authentication is needed.

Client private key filename

Browse to the file that contains the client’s private key that is used when certification is required.

  • Public Key Infrastructure in EcoStruxure Building Operation
  • Web Server Certificate Dialog Box – Basic Tab