earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Security
Product version: 2024, 7.0
2/22/2024

Configure the Certificate Agent Workflow

Use this workflow to configure the certificate agent on the EcoStruxure Building Operation server.

Related information can be found in the sections after the flowchart.

 
action_zoom_plus_stroke Configure the Certificate Agent Workflow
Figure: Configure the Certificate Agent Workflow
Configure the global certificate settings

All EcoStruxure Building Operations servers must be configured to connect to the PKI server using the EST protocol.

For more information, see Configuring Communication with the Enrollment over Secure Transport Server .

Configure the Web Server certificate settings

Enable the use of PKI on the EcoStruxure Building Operation server and add information to the Certificate Signing Request (CSR).

For more information, see Configuring the Global Certificate Settings .

  • Public Key Infrastructure in EcoStruxure Building Operation
  • Configuring Communication with the Enrollment over Secure Transport Server
  • Configuring the Global Certificate Settings