earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Produits : AS-B, Edge Server, AS-P
Fonctionnalités : Fonctionnalité de base
Version produit : 2024, 7.0
02/12/2024

Validation of Field Server Backups

Field server backups contain a checksum used to validate the backup when restoring. The validation is done to avoid that the backup has been tampered with.

When you restore a backup, the checksum is validated. You are notified if the validation fails by an error message. If you suspect that someone has tampered with the backup, you can abort the restore. If you are sure that no one has tampered with the backup, you can procced with the restore process.

Replacing a faulty field server with new hardware always result in checksum error. In this case it is acceptable to proceed with restore if there are no indications or suspicions that the backup has been tampered with.

  • Restore
  • Restoring the EcoStruxure BMS Server
  • Restoring a Field Server from the Enterprise Server