earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Концепт

Концепт


Продукты: AS-P-3
Функции: Аппаратное обеспечение
Версия продукта: 7.0
22.09.2025

AS-P-3 Server Screw Terminals

The AS-P-3 server models have removable (pluggable) screw terminal blocks on the top of the device. The terminal blocks are easy to install and remove from the device. The terminal blocks are delivered with the device.

Spare terminal blocks can be ordered separately using the part number SXWASPCON10002.

The wiring recommendations are provided separately. Более подробную информацию см. Wiring .

The recommendations for the RS-485 interface port configuration are provided separately. Более подробную информацию см. RS-485 Communications .

AS-P-3 Screw Terminals

The AS-P-3 model has four removable screw terminal blocks, one for the power input and three for RS-485 serial communications.

Более подробную информацию см. AS-P-3 Screw Terminals .

AS-P-L-3 Screw Terminals

The AS-P-L-3 model has four removable screw terminal blocks, one for the power input and two for RS-485 serial communications, and one for LonWorks communications.

Более подробную информацию см. AS-P-L-3 Screw Terminals .

  • AS-P-3 Servers
  • AS-P-3 Screw Terminals
  • AS-P-L-3 Screw Terminals
  • Wiring
  • RS-485 Communications