earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Пользовательский интерфейс

Пользовательский интерфейс


Продукты: AS-P-3
Функции: Аппаратное обеспечение
Версия продукта: 7.0
22.09.2025

AS-P-3 Server LEDs

arrow1_rotationStatus LED arrow1_rotationRS-485 LEDs arrow1_rotationEthernet LEDs arrow1_rotationLON LED

There are several LEDs on the front panel of an AS-P-3 server.

The AS-P-3 server comes in two different models, AS-P-3 and AS-P-L-3. Both models have seven LEDs.

 
action_zoom_plus_stroke  AS-P-3 model LEDs
Рисунок: AS-P-3 model LEDs
 
action_zoom_plus_stroke  AS-P-L-3 model LEDs
Рисунок: AS-P-L-3 model LEDs

Таблица: The Seven LEDs

Function

Color

RS-485 A, TX/RX

Yellow/Green

RS-485 B, TX/RX

Yellow/Green

RS-485 C, TX/RX a or

LON, TP/FT b

Yellow/Green or

Red

Ethernet 1, Link/Act/Speed

Green/Yellow/Orange

Ethernet 2, Link/Act/Speed

Green/Yellow

Ethernet 3, Link/Act/Speed

Green/Yellow

Status (AS-P-3 server)

Green/Red

  1. Only available on the AS-P-3 model.
  2. Only available on the AS-P-L-3 model.
Примечание

The RS-485, LON, Ethernet 2 and 3, and Status indicators comprise two LEDs (green/yellow and green/red respectively) in one structure. Normally, when one LED is lit, the other is not lit and vice versa, that is, the indicator will show one color at a time.

The LEDs indicate status of the device and the ongoing communication.

Status LED

The AS-P-3 server Status LED indicates the condition of the device.

Таблица: AS-P-3 Server Status LED Patterns

LED Patterns

Condition

Green, constant

Normal operation, status OK

Green, flashing

Device starting, wait

Red/green, flashing (~1 Hz)

Device firmware upgrade (DFU) mode or firmware being downloaded in DFU mode

Red, flashing (~1 Hz)

Device operates, but a problem needs attention

Red, constant

Detected error, attention required

No light

No input power

RS-485 LEDs

The RS-485 LEDs indicate the condition of the RS-485 communication.

Таблица: RS-485 LED Patterns

LED Patterns

Condition

Yellow, flashing

Transmit data (TX)

Green, flashing

Receive data (RX)

Ethernet LEDs

The Ethernet LEDs indicate the condition of the Ethernet communication.

Таблица: Ethernet LED Patterns

LED Patterns

Condition

Green, constant

10 Mbit communication a , link established

Green, flashing

10 Mbit communication a , activity on the port

Yellow, constant

100 Mbit communication a , link established

Yellow, flashing

100 Mbit communication a , activity on the port

Orange (amber), constant

1000 Mbit communication a , link established

Orange (amber), flashing

1000 Mbit communication a , activity on the port

  1. Ethernet 1 supports 10/100/1000 Mbit communication. Ethernet 2 and 3 support 10/100 Mbit communication.

LON LED

The LON LED indicates the condition of the LonWorks TP/FT communication.

Таблица: LON LED Patterns

LED Patterns

Condition

Red, constant

Detected error, attention required

Red, flashing (~1 Hz)

Non-configured node, attention required

No light

Normal operation, status OK

Примечание

Only the AS-P-L-3 model has a LON LED.

  • AS-P-3 Servers
  • Status LEDs