This section outlines the recommended cables and wires, specifying the appropriate wire sizes and lengths for the AS-P-3 servers.
For more information, see AS-P-3 Servers .
The recommendations are for guidance only. Other wire sizes and lengths may be used, depending on wiring rules and when appropriate.
|
Terminals |
Minimum Cross-sectional Area |
Maximum Cable Length |
|
Power input terminals (1, 2) |
0.75 mm² (18 AWG) a |
According to local wiring rules |
|
Functional earth ground terminal (3) |
0.75 mm² (18 AWG) a |
According to local wiring rules |
|
RS-485 terminals (4, 5, 6, 7, 8, 9, 10, 11 b , 12 b , 13 b ) |
For more information, see RS-485 Communications . |
For more information, see RS-485 Communications . |
|
LON terminals (11 b , 12 b , 13 b ) |
0.34 mm² (22 AWG) c |
1,400 m (4593 ft) c |