earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Концепт

Концепт


Продукты: RP-C, RP-C-EXT-0-10V-4, RP-C-EXT-0-10V-4-PD
Функции: Аппаратное обеспечение
Версия продукта: 3.2, 3.3, 2022, 2023, 2024, 7.0
05.07.2024

Wire Sizes and Lengths for the 0-10V Light Outputs of the RP Controller Expansion Light Modules

This section provides recommendations on wires sizes and lengths for the 0-10V Light outputs of the RP controller expansion light modules.

The recommendations apply to the following RP controller expansion light modules:

  • RP-C-EXT-0-10V-4-PD and RP-C-EXT-0-10V-4

The recommendations are for guidance only. Other wire sizes and lengths may be used, depending on wiring rules and when appropriate.

Таблица: Wire Sizes and Lengths for the 0-10V Light Outputs of the RP Controller Expansion Light Modules

Terminals

Minimum Cross-sectional Area

Maximum Cable Length

Light output terminals a for 0-10V lighting control

0.34 mm² (22 AWG)

100 m (330 ft)

  1. The Light output terminals are marked "AOn" (n: 1 to 4) and “COM”.
  • I/O Wiring
  • Wire Sizes and Lengths
  • RP-C Controllers
  • RP-C-EXT-0-10V-4-PD
  • 0-10V Light Outputs with Power Distribution
  • RP-C-EXT-0-10V-4
  • 0-10V Light Outputs without Power Distribution
  • Wire Sizes and Lengths for the Power Input and Power Output of the RP Controller Expansion Modules
  • Wire Sizes and Lengths for the Digital Inputs of the RP Controller Expansion Modules
  • Wiring