earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Концепт

Концепт


Продукты: WebStation
Функции: Dashboards
Версия продукта: 7.0
19.12.2024

Point Table

A point table is used to show one or more property values of objects.

You can show multiple variables of different objects in a point table. You can also present a summary in a row in the bottom of the widget. If all values of a column are the same unit category, the value in the summary is converted during calculation. For example, 1 kW + 100 W is converted to 1,1kW.

  • Dashboard Widgets
  • Configuring a Point Table