earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Comment faire pour

Comment faire pour


Produits : WebStation
Fonctionnalités : Dashboards
Version produit : 7.0
19/12/2024

Configuring a Point Table

You configure a point table to show a number of variables from different objects in a table for comparison.

Afficher plus
action_close

A point table is used to show one or more property values of objects.

You can show multiple variables of different objects in a point table. You can also present a summary in a row in the bottom of the widget. If all values of a column are the same unit category, the value in the summary is converted during calculation. For example, 1 kW + 100 W is converted to 1,1kW.

To configure a point table
  1. Right-click the dashboard and click Edit dashboard .

  2. Click Configure or click the Settings button

     
    action_zoom_plus_stroke
    .

  3. In the Point Settings properties dialog box, click Add .

  4. In the Select property dialog box, select the object you want to display.

  5. In the Column list, select a column you want to display. At least one column must be selected.

  6. In the Caption box, type a caption.

  7. In the Caption Link box, enter a link to an object that is relevant for the point pie.

  8. In the Decimal box, select the number of decimals to display.

  9. Click Add to add a guide to define the color for a value.

  10. In the Value column, enter the value.

  11. In the Color column, enter the color.

  12. In the Footer row , select if you want a calculation of the values.

  13. Click OK .

  • How Dashboards Work
  • Dashboard Widgets
  • Widget Dialog Box – Layout Tab
  • Adding a Widget to a Dashboard
  • Point Table