earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: Sustainability, 趋势
产品版本: 7.0
2024/12/19

Creating a Meter Hierarchy

A meter hierarchy is a view of relations between meter objects and meter processors.

显示更多
action_close

A meter hierarchy is a view of relations between meter objects and meter processors.

You can create a Sankey diagram from a meter hierarchy to help you analyze your energy consumption.

To create a meter hierarchy
  1. In WebStation, in the System tree , right-click a meter processor or a meter object.

  2. Click Create object , then click Meter Hierarchy .

  3. Edit the name and the path if required.

  4. Click OK .

  5. In the Meter Hierarchy view, in the Meter value list, select the meter value.

  6. Click the edit button

     
    action_zoom_plus_stroke
    .

  7. Configure the meter hierarchy view.

    有关更多信息,请参阅 Meter Hierarchy View .

  8. Click OK .

  • Meter Hierarchy
  • Meter Hierarchy View