earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: WebStation
功能: 基本功能
产品版本: 7.0
2024/12/19

Editing a Text File Using WebStation

You can edit a text file to keep it updated.

显示更多
action_close

You can open documents stored on an EcoStruxure BMS server using the default program associated with the file type. For example, a txt-file opens Notepad and a ppt-file opens PowerPoint.

You can edit the documents and then save them again using WorkStation. You cannot edit and save documents using WebStation.

重要:

When you log off or are automatically logged off, any unsaved changes in the document are not saved in the database. Make sure that you save changes in open documents frequently.

To edit a text file using WebStation
  1. In WebStation, in the System Tree pane or List view, click the text file you want to edit.

  2. Edit a .txt file by writing in the text area. Click Save .

You can only edit the text file you have access to.

  • Basic Functions
  • How Documents Work
  • Opening a Document