earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Pojęcie

Pojęcie


Produkty: WorkStation, WebStation
Funkcje: Podstawowa funkcjonalność
Wersja produktu: 2022, 2023
2024-09-18

HTML Utilities

The HTML utility object enables experienced software developers to embed custom web pages/applications inside the system.

The attached HTML file should inline it's CSS and be self-contained.

There is a possibility to access external data through the security setting "Lists external websites that are allowed to be embedded in WebStation." That setting will lower the security generally for WebStation and open the CSP default-src against the domain(s) you specify.

See https://developer.mozilla.org/en-US/docs/Web/HTTP/CSP for more information.

Więcej informacji zawiera Configuring Security in WebStation using WorkStation .

Więcej informacji zawiera Configuring Security in WebStation using WebStation .

Uwaga

Note that the checkbox option "Enable external websites to be embedded into WebStation" lowers the security significantly. Do not use these settings if you do not understand the security implications. Both these settings are related to how external data can be accessed and integrated on the client side. Web browser vendors continuously strengthen cybersecurity and may deprecate the possibility in the future. We do not recommend using any of these options, as future sandboxing of the HTML utility might block all such external access.

  • Utilities
  • Configuring Security in WebStation using WebStation
  • Configuring Security in WebStation using WorkStation