earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: WorkStation, WebStation
功能: 基本功能
产品版本: 2024, 7.0
2024/12/2

HTML Utilities

The HTML utility object enables experienced software developers to embed custom web pages/applications inside the system.

The attached HTML file should inline it's CSS and be self-contained.

There is a possibility to access external data through the security setting "Lists external websites that are allowed to be embedded in WebStation." That setting will lower the security generally for WebStation and open the CSP default-src against the domain(s) you specify.

See https://developer.mozilla.org/en-US/docs/Web/HTTP/CSP for more information.

有关更多信息,请参阅 Configuring Security in WebStation using WorkStation .

有关更多信息,请参阅 Configuring Security in WebStation using WebStation .

重要:

Note that the checkbox option "Enable external websites to be embedded into WebStation" lowers the security significantly. Do not use these settings if you do not understand the security implications. Both these settings are related to how external data can be accessed and integrated on the client side. Web browser vendors continuously strengthen cybersecurity and may deprecate the possibility in the future. We do not recommend using any of these options, as future sandboxing of the HTML utility might block all such external access.

  • Utilities
  • Configuring Security in WebStation using WebStation
  • Configuring Security in WebStation using WorkStation