Use the Options dialog box - Builder Settings to manage exposed properties settings in Builder View.
Component |
Description |
Edit |
Click to edit which canvas object properties preferences you want to expose. For more information, see Preferences: Exposed Properties Dialog Box . |
Import |
Click to import preferred exposed properties. The imported preferences will be added to your existing saved preferences. For more information, see Preferences: Exposed Properties Dialog Box . |
Export |
Click to export your existing saved preferred exposed properties to be able to share them with other users. For more information, see Preferences: Exposed Properties Dialog Box . |
Reset |
Click to remove all your existing saved preferred exposed properties and to reset them back to the original default exposed properties. For more information, see Removing Exposed Properties Preferences . |