earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Koncept

Koncept


Produkter: Enterprise Central, Enterprise Server, Project Configuration Tool
Funktionaliteter: Lokalisering
Produktversion: 2024, 7.0
2024-12-11

FDP Server Time and Time Zone Configuration

​The FDP server gets its date and time from the FDP panel operating system and are configured in Fire Expert. The time zone offset is configured in the FDP server using Workstation and is added to the FDP panel UTC time by the EcoStruxure Fire Operation software. The FDP panel operating system time zone settings are independent of the FDP server time zone settings.

 
action_zoom_plus_stroke  The FDP server uses the FDP panel operating system clock. Time zone offset and DST are added to the UTC time by the EcoStruxure Fire Operation software.
Figur: The FDP server uses the FDP panel operating system clock. Time zone offset and DST are added to the UTC time by the EcoStruxure Fire Operation software.

The FDP panel operating system clock is adjusted in Fire Expert. Mer information finns i O1891 EcoStruxure Fire Expert Configuration Manual ..

  • Time and Time Zone Overview
  • Time Zone Settings Synchronization
  • Creating a FDP Server Custom Time Zone
  • Changing a FDP Server Time Zone