earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 本地化
产品版本: 2024, 7.0
2024/12/3

Creating a FDP Server Custom Time Zone

You create a FDP server custom time zone if the required time zone is not predefined.

显示更多
action_close

​The FDP server gets its date and time from the FDP panel operating system and are configured in Fire Expert. The time zone offset is configured in the FDP server using Workstation and is added to the FDP panel UTC time by the EcoStruxure Fire Operation software. The FDP panel operating system time zone settings are independent of the FDP server time zone settings.

 
action_zoom_plus_stroke  The FDP server uses the FDP panel operating system clock. Time zone offset and DST are added to the UTC time by the EcoStruxure Fire Operation software.
图: The FDP server uses the FDP panel operating system clock. Time zone offset and DST are added to the UTC time by the EcoStruxure Fire Operation software.

The FDP panel operating system clock is adjusted in Fire Expert. 有关更多信息,请参阅 O1891 EcoStruxure Fire Expert Configuration Manual ..

To create a custom time zone of an EcoStruxure BMS server
  1. In WorkStation, in the System Tree pane, expand the FDP server you want to create a custom time zone for.

  2. Expand System and then select Time Settings .

  3. On the Zone Info tab, create a custom time zone.

  • FDP Server Time and Time Zone Configuration
  • Changing a FDP Server Time Zone