earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Builder for Function Block
Functionalities: Engineering
Product version: 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024, 7.0
1/24/2025

Function Block Program - Retain Versus Backup

Cold Start Retain (Public)

Typically, it is not possible to set the retain level for the values/signals in a Function Block program in the same way as you do for a system object, such as an analog value. For more information, see Retain Level .

For some blocks though, the retain level can be set to cold start if they are made public in the Inspector. For more information, see Property Inspector Pane .

You can set the retain level to cold start for the blocks and public constants in the table list below if they are made public. The list differs between server Function Block program and device Function Block program. The reason is that when you download a Function Block program and related objects to a device, you do not want to overwrite the values currently used in the device.

Table: Cold start retained when public

Block Name

Server

Device

BI

Yes

Yes

BO

Yes

No

RBO

Yes

No

II

Yes

Yes

IO

Yes

No

RIO

Yes

No

PI

Yes

Yes

PO

Yes

No

RI

Yes

Yes

RO

Yes

No

RRO

Yes

No

NCYC

Yes

No

PVB

Yes

Yes

PVI

Yes

Yes

PVR

Yes

Yes

SHB

Yes

No

SHI

Yes

No

SHR

Yes

No

FILT

Yes

No

RAMP

Yes

No

ACUM

Yes

No

INTEG

Yes

No

RT

Yes

No

Constants

Yes

Yes

Warm Start Retain (Backup)

Function block objects have their own backup function. The backup function in Function Block overrides the retain level in EcoStruxure BMS for a warm start. For more information, see Edit Block Dialog Box .

Server

When a warm start is performed on a server, the Function Block objects themselves determines the start value to set in the end. This is done regardless of the set Backup status, and it also overrides any retain level set to cold start. The Function Block object sets the value to the initial value, if such a value exists, when the Backup function is not selected.

Device

When a warm start is performed on a device, as opposed to on a server, the Function Block objects do not override any retain level set to cold start when the Backup function is not selected.

  • Retain Level
  • Property Inspector Pane
  • Edit Block Dialog Box